AnsweredAssumed Answered

Android O8.0.0_1.0.0  can not boot up on iMX6dl

Question asked by lu winbo on Jun 1, 2018
Latest reply on Nov 17, 2018 by crl6 crl6

Hi, 

 

Android O8.0.0_1.0.0  can not boot up on iMX6dl, The boot up log looks like as following.

 

init: Service 'surfaceflinger' (pid 268) exited with status 1
init: Sending signal 9 to service 'surfaceflinger' (pid 268) process group...
init: kill(-268, 9) failed: No such process
init: Successfully killed process cgroup uid 1000 pid 268 in 4ms
init: Sending signal 9 to service 'zygote' (pid 252) process group...
init: Successfully killed process cgroup uid 0 pid 252 in 16ms
init: Service 'zygote' (pid 252) killed by signal 9
init: Unable to open '/sys/android_power/request_state': No such file or directory
init: Unable to write to '/sys/power/state': Invalid argument
init: Sending signal 9 to service 'audioserver' (pid 272) process group...
init: Service 'surfaceflinger' (pid 361) exited with status 1
init: Sending signal 9 to service 'surfaceflinger' (pid 361) process group...
init: kill(-361, 9) failed: No such process

....

imx2-wdt 20c0000.wdog: Device shutdown: Expect reboot!
reboot: Restarting system with command 'recovery'
imx2-wdt 20c0000.wdog: failed to assert external reset, trying with timeout
Reboot failed -- System halted

 

The detail log please refer to the attachment.

Is there any suggestion? Thanks for your helps.

 

Winbo

Attachments

Outcomes