AnsweredAssumed Answered

QN9080-DK drivers on host PC (Windows)

Question asked by Sanghamitra Bhattacharya on May 31, 2018
Latest reply on Jun 6, 2018 by Sanghamitra Bhattacharya

I am trying to connect and use the QN9080-DK and program it with one of the SDK examples (beacon). However, the drivers not getting installed properly on my Windows PC. I followed the instruction in the QN908x Quick Start Guide Chapter 4, but do not see the devices in the Device Manager as shown in Fig 4. I've tried both on Windows 7 and Windows 10. What do I need to do to ensure device drivers are installed corrrectly? I've tried with MCUXpresso v 10.1.1 and MCUXpresso IDE v10.2.

 

The drivers for the virtual COM port for the BLE dongle are also not installed correctly (see attachment 2)

Outcomes