MTRDEVKSBNK144 PreDRV Fault

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MTRDEVKSBNK144 PreDRV Fault

991 Views
sohyunjang
Contributor III

Hi, I use MTRDEVKSBNK144.

I test the board, but PreDRV Fault was occurred.

tppDrvConfig.deviceConfig.statusRegister[0U] = 8

tppDrvConfig.deviceConfig.statusRegister[1U] = 73

tppDrvConfig.deviceConfig.statusRegister[2U] = 255

tppDrvConfig.deviceConfig.statusRegister[3U] = 0

I just connected the power(12V, 1.5A adapter), not run motor.

WhatWhat's problem??

Thank you.

Labels (1)
0 Kudos
1 Reply

544 Views
Eugene3957
Contributor I

I figured it out it was due to wrong pin settings.
try to use J107 1-2 (use 12 v)

0 Kudos