Hello, I am relatively new to working with the board and ZigBee in general.
I have flashed the Zigbee 3.0 router example into the KW41Z and pressed SW3 to attempt to join the network formed from my computer with the XBee Pro S2C serving as the coordinator. The KW41Z detected the network but it throws an error "FailedToJoin sNwkJoinFailedEvent.u8Status=173.", which I have no idea how to get over.
Any help would be highly appreciated.
Hello,
By any chance, have you verified you followed all the steps on how to form a network as it is mentioned on the ZigBee 3.0 Base Device Template pdf document section 4.3 Using the Router page 8?
Regards,
Estephania
Hello Estephania,
Sorry for the late reply but I have followed the instructions in that document, but it has occurred to me that my XBee module uses ZigBee PRO, not exactly ZigBee 3.0. Is there a way to make these two compatible with each other? Or do I need to use Zigbee 3.0 XBee modules?
Thanks
Hello,
ZigBee 3.0 employs the ZigBee PRO protocol so there should be no issue regarding that. You could check the ZigBee 3.0 Stack document for more details about this.
Regards,
Estephania
Yes, I found that out soon after I made that reply.
Could you explain what "sNwkJoinFailedEvent.u8Status=173" means in this case? The documentation seems to point this error to "ZPS_APL_APS_E_SECURITY_FAIL", but I am not quite sure what is causing the security processing issue.