AnsweredAssumed Answered

h264 files bounded to 2 Go

Question asked by Christophe Cholet on May 30, 2018
Latest reply on May 31, 2018 by igorpadykov

Hi all,

 

We have a imx6q platform under yocto (L4.1.15_1.0.0). We used to recording h264 files with it onto sd cards (without gstreamer).

Today, we want to create big record files (>10 Gb). But we observe a limitation of 2 Gb. Even if the recorded sequence is superior to 2Gb, when closing the file, it is truncated at 2 Gb. It's very curious because the sd card is a fat32 one, so at least 4 Gb are expected. It's clearly not our application that is in concern. We suppose it's due to linux system configuration, but where...

 

Do you have some suggestions about this issue ?

 

Rgds,

Christophe

Outcomes