PCA9701 and PCA9702

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCA9701 and PCA9702

Jump to solution
735 Views
sasa_mesaric
Contributor I

Hi !

we are using PCA9701 and PCA9702.

Datasheet says :

Multiple PCA9701 or PCA9702 devices can be serially connected for monitoring a large number of switches by connecting the SDOUT of one device to the SDIN of the next device. SCLK and CS must be common among all devices and interrupt outputs may be tied together. No external logic is necessary because all the devices’ interrupt outputs are open-drain that function as ‘wired-AND’ and can simply be connected together to a single pull-up resistor.

Does this mean that we can connect  one PCA9701 and one PCA9702 together like described above or only PCA9701 can be connected together with another PCA9701 (same goes for PCA9702), so combination of PCA9701 and PCA9702 is not allowed?

Thank you !

Regards !

0 Kudos
1 Solution
648 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi,

This mean you can mixed connect PCA9701 and PCA9702 together.

View solution in original post

0 Kudos
2 Replies
649 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi,

This mean you can mixed connect PCA9701 and PCA9702 together.

0 Kudos
648 Views
sasa_mesaric
Contributor I

Thank you !

0 Kudos