Hi, I'm working with an SBC8548 eval board and am trying to get some very basic setup code written for the processor. In particular I'm looking at TLB's at the moment and to start with I was going to set them up the same as the CW target initialisation script I've been using to flash the board. However in the script it uses the writereg128 command as follows: -
From the help file it says that this command combines the 4 32 bit values and writes them to the specified 128 bit TLB registers. Now looking at the 8548 reference manual I can see that there are the MASx registers used to setup the TLB so I assumed the command would write to the MAS0-3 registers and then execute a tlbw command but the values in the above command don't seem to correlate to the bit definitions of those registers at all? So where exactly does the writereg128 command put those values?