API documentation for drivers in MCUXpresso SDK - where is it located?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

API documentation for drivers in MCUXpresso SDK - where is it located?

1,195 Views
russelleverett
Contributor I

API documentation for drivers in MCUXpresso SDK - where is it located?

2 Replies

642 Views
BlackNight
NXP Employee
NXP Employee

With MCUXPresso IDE 10.2 (see as well Overview of MCUXpresso IDE v10.2.0 | MCU on Eclipse ) you have direct access to the API documentation and more if you click on the SDK installed, for example the SDK API Reference manual:

pastedImage_1.png

I hope this helps,

Erich

642 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Russell Everett,

About the new MCUXpresso SDK package ,  API description is in driver header files,

for example driver ADC , find header file under SDK package : SDK_2.3.1_FRDM-K82F\devices\MK82F25615\drivers\fsl_adc16.h

pastedImage_1.png

Hope it helps


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos