AnsweredAssumed Answered

Not able to flash through OPENSDA

Question asked by Ambarish Hundekar on May 28, 2018
Latest reply on Jun 6, 2018 by Diana Batrlova

Hello,

 

I am using S32K144 evaluation board.

power up the board and flashing through USB .

 

Earlier I was able to do flashing, but now not able to flash.
The red led next to the USB stays on, and the board will not enter boot loader mode when powered with reset button pressed.


RGB LEDS are continuously glowing but not able to connect to the board via OpenSDA Interface.

I clicked on the debug in S32 design studio , Open SDA window opens and ask for the Open SDA USB port , if I click on Retry also , again and again it is asking the same (Retry option).


Thank you in advance for your help.



Regards,
Ambarish









Outcomes