eth0 is not ready I.mx6ull EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

eth0 is not ready I.mx6ull EVK

538 Views
建洪徐
Contributor I

Hello

   boot:dhcp:

From ifconfig, both interfaces have same MAC addresses, but no IP addresses although the interfaces are configured for

DHCP:

The status LEDs on the ethernet ports are not even on. 

Any thoughts on how to fix this issue?

 

pig1.pngpiture2.png

Labels (3)
0 Kudos
3 Replies

399 Views
joanxie
NXP TechSupport
NXP TechSupport

try to use "ifconfig eth0 address" to set the eth0 ip address, then in the uboot, use "setenv serverip address" this adress is same as eth0

0 Kudos

399 Views
建洪徐
Contributor I

Thank you for your advice!

   Follow the method you provided,then in the uboot,"setenv ipaddr 192.168.1.59",But after entering the Linux, there is still no IP address.

The final question is that the eht0 and eth1  is not link.The status LEDs on the ethernet ports are not even onlink.png

ip.png

0 Kudos

399 Views
joanxie
NXP TechSupport
NXP TechSupport

I mentioned that you need to set the same serverip as eth0, not ipaddr

0 Kudos