AnsweredAssumed Answered

No Commissioning/Joining between JN5168 DimmableLight and JN5168 ControlBridge

Question asked by Georgi Radkov on May 27, 2018
Latest reply on Jun 17, 2018 by layengchan

Hello,

I need some help with JN5168 commissioning/Joining

 

Here is my setup:
- Using 2 x JN5168-001-M00
- Programmer - ft232rl - no problems with programming
- all needed LEDs and Switches from DR1175 and DR1174 (DIO8, RESETN, WhiteLeds(PWM))

 

- First JN5168 module is programmed with "JN-AN-1216-Zigbee-3-0-IoT-ControlBridge"
                              -> "ZigbeeNodeControlBridge_JN5168_FULL_FUNC_DEVICE_1000000.bin"

 

- Second JN5168 module is programmed with BeyondStudio compiled "DimmableLight_JN5168_DR1175.bin" from "JN-AN-1218-Zigbee-3-0-Light-Bulb"

 

Here is the problem:

 

I start ControlBridge and set all configs according to "JN-AN-1216-ZigBee-3-0-IoT-ControlBridge-UserGuide" or

"HMB-N1983 Hands-On Workshop"
- Set CMSK = 20
- Set EPID = 0
- Set Type = Coordinator
- Start NWK
- Permit Join = "0 and FF" or "FFFC and FE" according to UserGuide's

 

Then RESET "DimmableLight" and "DimmableLight" is sending this via UART:

 

Stack low water mark is at 04006c78
***********************************************
* LIGHT NODE RESET *
***********************************************
APP: Entering APP_vInitResources()
APP: Initialising resources...
APP_vInitialiseNode

Zll recovered state 00

Set a random pan

Factory new start up
PDM: Capacity 27
PDM: Occupancy 36
APP: Entering BDB_vStart()
APP: Entering APP_vMainLoop()
APP: BDB No Networks
APP: BDB No Networks -> Wait On 11

It is strange that there is Coordinator but no Networks and "DimmableLight" can't connect to network.
The Coordinator isn't showing anything about new device. Discover Devices doesn't find any devices. Start Scan also.

This Response isn't showing


Some Testings I've made:

- ControlBridge is finding only "AN1229_ZBP_SleepingEndDevice_JN5168" device from "ZigBee PRO Application Template for ZigBee 3.0"
- All JN-AN-1217-Zigbee-3-0-Base-Device are working perfectly with "DimmableLight" devices

 

So Please give me a hint how to Join DimmableLight to ControlBridge

Thanks

Outcomes