May I know how can I program a .axf file into MKL27z128VFT4?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

May I know how can I program a .axf file into MKL27z128VFT4?

2,592 Views
ecang
Contributor I

I have an USB-Multilink Universal flash programmer and an AXF file.  Please advice how can I perform flash programming of .AXF file into NXP MKL27z128VFT4 ?

mkl27z #AXF file programming usb multilink universal    #flash programming‌

0 Kudos
1 Reply

558 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi EC ANG,

    Do you have the .axf project with IDE? If you use the IDE, it can downloaded the project with the Mutlilink.

    But if you want to download the .axf, .hex, .bin file with the PE multilink directly without the IDE, you need to use the P&E's  specific software:

PEmicro - P&E Microcomputer Systems: Over 30 years as an Industry leader in Embedded Systems Develop... 

    More details, you need to check it with the P&E engineer.

    If you use the IDE project, it will be very simple, you just need configure the debugger interface as P&E Multilink.

Wish it helps you!

If you still have question about it, please kindly let me know!

   

   


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos