AnsweredAssumed Answered

ov5642 30fps not working

Question asked by Jamal Mohiuddin on May 24, 2018
Latest reply on Jun 5, 2018 by Jamal Mohiuddin

Hi Guys,

 

We have a customized i.MX6Q Board based on sabrelite reference board.

 

We have the following configuration:

Linux : 3.10.53

Gstreamer 1.0 latest i.MX6 Plugins

 

We connected OV5642 Camera over CSI Interface..Used the following command to display the camera output on the screen.

 

gst-launch-1.0 imxv4l2videosrc device=/dev/video0 imx-capture-mode=4 fps-n=15 ! imxipuvideosink

 

It works, but initially, it takes time to settle for few seconds,  there is genlock issue 

 

But when I modify the fps to 30, I get distorted output.. What do you think is wrong here.. Any help is appreciated... 

 

 

The problem is not with OV5642, as it works well when I connect it to Boundary devices reference board at 30fps.

 

Thanks,

Jamal

Outcomes