eDMA channel idle

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

eDMA channel idle

425 Views
martindusek
Contributor V

Hi,

how to check whether a dma channel is free to execute new DMA request? I thought about using ACTIVE and DONE bits of CSR register, but it seems they are not suitable for that.

Checking DONE == 1 works only when there was previous DMA transaction (it doesn't work if the DMA channel hasn't been used yet).

And ACTIVE is set to 0 on minor loop completition. I want something that tells me all major loops (whole tranaction) has been completed.

Thanks for help.

Labels (1)
0 Kudos
2 Replies

327 Views
mjbcswitzerland
Specialist V

Hi

You could do a single dummy transfer during system initialisation in order to prepare the DONE bit and then use it as flag during subsequent operations.

Regards

Mark

0 Kudos

327 Views
martindusek
Contributor V

Hi Mark,

thanks. I'll do it If this is the only possibility...

0 Kudos