Hello BP,
It would seem that, for many of the older HC908 devices, the minimum value for "POR rise time ramp rate" is specified within the datasheet, usually either 20 V/s or 35 V/s. However, this specification seems to have been omitted within the HCS08 device datasheets.
For the HC908's, there is also a further requirement to which Kef was alluding.
If minimum V DD is not reached before the internal POR reset is released, the LVI will hold the part in reset until minimum Vdd is reached.
For the 'LC60 device, low voltage reset is enabled on occurrence of POR. Just in case a voltage dip is not sufficient to cause POR, leaving LVI reset enabled should give better reliability for these circumstances.
Regards,
Mac