AnsweredAssumed Answered

i.MX6Quad - GPIO settings in Yocto OS source files

Question asked by mocfur13 on May 23, 2018
Latest reply on May 24, 2018 by igorpadykov

Hi,

 

I'm working on the Digi ConnectCore6 SBC and trying to set some GPIOs to the different state from the default setting defined in Digi Embedded Yocto (DEY). ConnectCore6 has i.mx6 quad and DEY's version is yocto2.2/linux4.1. As I booted up the SBC and confirmed the state of GPIO198 on the /sys/kernel/debug with serial console,  it showed below,

 

root@ccimx6sbc:/sys/kernel/debug# cat gpio
GPIOs 0-31, platform/209c000.gpio, 209c000.gpio:
gpio-2 (can_stby ) out lo
gpio-5 (can_stby ) out lo
gpio-25 (phy-reset ) out lo

 

GPIOs 32-63, platform/20a0000.gpio, 20a0000.gpio:
gpio-34 (sysfs ) in lo
gpio-35 (sysfs ) in hi
gpio-36 (sysfs ) in hi
gpio-57 (aud_pwr_en ) out lo
gpio-58 (uart-pwr-en-gpio ) out lo
gpio-62 (spi_imx ) out lo

 

GPIOs 64-95, platform/20a4000.gpio, 20a4000.gpio:

 

GPIOs 96-127, platform/20a8000.gpio, 20a8000.gpio:
gpio-106 (spi_imx ) in lo

 

GPIOs 128-159, platform/20ac000.gpio, 20ac000.gpio:

 

GPIOs 160-191, platform/20b0000.gpio, 20b0000.gpio:
gpio-171 (? ) out lo

 

GPIOs 192-223, platform/20b4000.gpio, 20b4000.gpio:
gpio-198 (sysfs ) out lo

 

GPIOs 240-255, da9063-gpio, can sleep:
gpio-247 (gpio-ext-reg ) out hi

 

 

And when I measured the voltage of the corresponding pin (connected to open header), it was 3.3V. So the setting is guessed as "out high". I'd like to set the GPIO198 to "input"  durning the booting sequence of Yocto OS (like the initializing sequence of MCU). What kind of source flies should I modify and how should I modify it with the above settings before OS build?


I've already researched and tested about how to change the pinmux by modifying the .dtsi file before OS build, and how to manipulate the GPIOs with /sys/class/gpio APIs after OS boot. But I've not found the solution to modify the GPIO setting in the OS sources.


Any help is appreciated.


Best reards,

Outcomes