Hello,
I've just downloaded last MCUXpresso 10.2.0 release. Should I uninstall previous 10.1.1 version? Can I install 10.2.0 along 10.1.1?
Regards,
gaston
Solved! Go to Solution.
Hi Gaston.
You can have both MCUXpresso 10.2.0 and MCUXpresso 10.1.1 installed in your computer parallel.
You don't need uninstall 10.1.1.
On my side, both of these two versions are installed in my computer.
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
You'd think so wouldn't you! But when I installed 11.3.1 on Ubuntu it kindly deleted the previous install. Even though its in a separate appropriately named directory. Thank you NXP now I cant build my old projects without a reinstall and reinstalling all the SDKs too!
Hi All,
What to do if I would like to have the MCUXpresso v10.1.0 updated automatically to the latest version 10.2.1? What software site should I add for the automatic updates? For now, Check for Updates function returns "no updates found" for me. I assume there should be a software site to add in the list.
Hi Dmitry,
There is no update can update MCUXpresso IDE from 10.1.0 to 10.2.1.
MCUXpresso v10.2.1 is a standalone IDE package, you need download it from our website and install it separately.
MCUXpresso IDE|Eclipse-based Integrated Development Environment (IDE)|NXP
If you don't need MCUXpresso IDE 10.1.0 any more, you can uninstall it directly.
Have a great day,
TIC
Hi Gaston,
as Jennie outlined: you don't have to remove any previous version, just make sure you are installing it into a different directory (which is the default anyway). On another note: make sure you are *not* sharing/using workspaces between versions of the IDE. See as well Overview of MCUXpresso IDE v10.2.0 | MCU on Eclipse about this. This is not specific to MCUXpresso IDE, this is 'an Eclipse thing'.
I hope this helps,
Erich
Hi Gaston.
You can have both MCUXpresso 10.2.0 and MCUXpresso 10.1.1 installed in your computer parallel.
You don't need uninstall 10.1.1.
On my side, both of these two versions are installed in my computer.
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------