Hi All,
I'm having an old Codewarrior 8.3 DSC project I opened it in Codewarrior 8.3 itself using File-> Open. I was told that processor expert is suspended for this project so I selected "No" If I want to use Processor expert. After compiling and Building the project I'm getting a warning "The symbol Cfg_StartDelay was forced in the link with a "FORCE_ACTIVE" clause but no definition could be found". When I'm trying to debug I'm getting a window which says "CCSProtocolPlugin:Unknown Protocol Error". Can I know what may be problem. Please help me in this regard.
I'm using windows 7 32 bit operating system and USB TAP.
Hi Khalaque Abdul,
Regarding to the linking warning, check if Cfg_StartDelay is defined globally in source code.
connection error, check similar question and answer here:
CCSProtocolPlugin:Unknown protocol error
Note, officially CW8.3 doesn't support windows7, if above can't fix your connection issue. I suggest you try CW11
create a new project with CW11, test if it can connect board well.
I know some customers have ever worked with CW for DSC v8.3 on win7/10 by replacing "CodeWarrior for DSC56800E v8.3\ccs" folder with "CW MCU v11.0\MCU\ccs" folder. You can try it too.
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------