Is there a way to wake up IMX6Q via ethernet interrupt?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there a way to wake up IMX6Q via ethernet interrupt?

Jump to solution
747 Views
gkt
Contributor II

Hello all.

I am testing the sleep modes of IMX6QSABRESD. I can wake up the processor by using UART interrupt as it is mentioned in the Linux Reference Manual.

However, is there a way to wake up IMX6Q processor by using ethernet interrupt? 

Thank you in advance.

Labels (2)
0 Kudos
1 Solution
603 Views
igorpadykov
NXP Employee
NXP Employee

Hi Giray

please check patch on

Wake on lan in mx6 sabresd board 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
604 Views
igorpadykov
NXP Employee
NXP Employee

Hi Giray

please check patch on

Wake on lan in mx6 sabresd board 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------