AnsweredAssumed Answered

imx6ull 通过mfgtools刷新后无法启动

Question asked by 勇 纪 on May 21, 2018
Latest reply on May 21, 2018 by Rita Wang

提示信息为:

CPU:   Freescale i.MX6ULL rev1.0 528 MHz (running at 396 MHz)
CPU:   Commercial temperature grade (0C to 95C) at 49C
Reset cause: POR
Board: MYS-MX6ULL 14x14
I2C:   ready
DRAM:  256 MiB
NAND:  256 MiB
MMC:   FSL_SDHC: 0
*** Warning - bad CRC, using default environment
Display: TFT43AB (480x272)
Video: 480x272x24
In:    serial
Out:   serial
Err:   serial
Net:   FEC0
Error: FEC0 address not set.
Normal Boot
Hit any key to stop autoboot:  0
=> (?at 396 MHz
Unknown command '(?at' - try 'help'
不知道这是什么原因造成的。

Outcomes