MIPI CSI-2 iMX6DL Clock and Bayer 10

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIPI CSI-2 iMX6DL Clock and Bayer 10

1,388 Views
natesigrist
Contributor III

Does the IPU_CSI0_SENS_CONF[CSI0_SENS_PRTCL] need to be set?  Does it refer to the MIPI Clock coming from the camera.  For instance, the OV5675 can be programmed to gate the MCP/MCN when no data is transmitted.  Of does this refer to some internal signal?

Is this accurate for Bayer 10-bit,

1920x1080 (pixels/frame) x 10 (bits/pixel) / 8 (bits/cycle) x30 (frames/second) x 1.35 = 105 MHz;

I can't seem to force an EOF - does anyone have any ideas why that might be?

My [mostly] complete configuration is described here.

Labels (4)
Tags (2)
2 Replies

920 Views
natesigrist
Contributor III

Why oh why is this marked assumed answered!?!?1

0 Kudos

920 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nate

MIPI  usage is described in AN5305 MIPI–CSI2 Peripheral on i.MX6 MPUs

https://www.nxp.com/docs/en/application-note/AN5305.pdf 

MIPI CSI2 data transferred from MIPI CSI to IPU Gasket to IPU CSI and it is always

in non-gated clock mode. Bayer  example can be found on

i.MX6 OV5647 Bayer sensor driver (ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0) 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos