AnsweredAssumed Answered

kPollAbortTimeoutMs param value in Kinetis Bootloader package

Question asked by Vyacheslav Guzhva on May 17, 2018
Latest reply on Jun 14, 2018 by Jing Pan
  • Inside NXP Tool from Kinetis Bootloader package there default waiting time = 100ms after each command of writing via USB HID protocol. Such waiting time set into UsbHidPeriferals.h file
    • kPollAbortTimeoutMs = 100
  • But in this case whole bootloader (19KB) loading during ~1,5 minutes, which is not acceptable from mass production point of view.
  • can you recommend the most efficient parameter of waiting time for kPollAbortTimeoutMs (to have lower failed rate~=0,2%, but still with acceptable loading time)?

Outcomes