MPXH6250A6U

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPXH6250A6U

598 Views
raphaelleden
Contributor I

hello, in the data sheet there is no information with the cleaning compatibility.

Is it possible to wash the component with aqueous machine ?

how many cycle we can clean it ?

wich type of cleaning we can used ?

Labels (1)
0 Kudos
1 Reply

448 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Raphael, 

The following information is given in the AN3150:

The use of a No-Clean (NC) flux is recommended for exposed cavity components. Using pressure spray or other methods of cleaning is not recommended. If cleaning of the pcb is performed Water Soluble (WS) flux can be used, but it is recommended the component cavity to be protected by adhesive Kapton tape, vinyl cap or other means prior to the cleaning process to prevent contamination and foreign materials from being introduced into device cavity as result of cleaning processes.

Best regards,

Tomas

0 Kudos