AnsweredAssumed Answered

FLEXIO as SPI configuration

Question asked by Gaston Schelotto on May 15, 2018
Latest reply on Jul 9, 2019 by Hy Mai

Hi,

 

I'm evaluating FLEXIO as SPI using SDK v3.2.1 on a FRDM-KL27Z. Basically I'd need to solve 2 things:

  • Set the CLK Polarity Active Low, not High as provided in the frdmkl27z_driver_examples_flexio_flexio_spi_int_spi_transfer_master
  • Disable CS assertion by the driver. I need to set/clear the CS manually. Similar way than the output mode configuration (kSPI_SlaveSelectAsGpio) in the SPI driver.

 

How can I do to accomplish these points?

 

regards,

gaston

Outcomes