Port IRQ on S32V234

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Port IRQ on S32V234

2,382 Views
rolanddorn
Contributor II

Hi,

I wan't to generate a PORT IRQ. I configured the desired PIN and IRQ settings in SIUL2. After triggering the PIN from outside, the corresponding flag in SIUL2.DISR0 is set but the ISR function is not called.

Input PIN:                              PA5

MSCR of Input PIN:                5

Used alternative of input PIN:  2 -> EIRQ[5]

The sample code is running on the cortex M4.

At position 86 of the vector table the PORT ISR function is placed.

The IRQ is routed to cortex M4 : MSCM.IRSPRC[86-16].R = 0x1;

Does anyone have an idea or some tips what can be wrong?

Configuration of PORT IRQ:

        /* Mask interrupts by clearing the EIREn bits in DIRER0 */
        ClrBit(SIUL2, DIRER0, DIRER0_EIRE5);

        /* Rising-edge event is enabled */
        SetBit(SIUL2, IREER0, IREER0_IREE5);

        /* Falling-edge event is enabled */
        //SetBit(SIUL2, IFEER0, IFEER0_IFEE5);

        /* Disable Output Buffer */
        ClrBit(SIUL2, MSCR[5], MSCRx_OBE);

        ClrBit(SIUL2, MSCR[5], MSCRx_ODE);

        /* Enable Input Buffer */
        SetBit(SIUL2, MSCR[5], MSCRx_IBE);

        /* Set alternative */
        SetBitField(SIUL2, MSCR[5], MSCRx_MUX_MODE, 2);

        /* Daisy bit of SIUL2_IMCR#. */
        SetBitField(SIUL2, IMCR[83], IMCRx_DAISY, 2);

        /* Interrupt request is selected */
        ClrBit(SIUL2, DIRSR0, DIRSR0_DIRSR5);

        /* Filter Counter setting */
        SetBitField(SIUL2, IFMCR[5], IFMCRx_MAXCNT, 2);

        /* Filter Clock Prescaler */
        SetBitField(SIUL2, IFCPR, IFCPR_IFCP, 6);

        /* Enable digital glitch filter on the interrupt pad input. */
        SetBit(SIUL2, IFER0, IFER0_IFE5);

        SetBit(SIUL2, DISR0, DISR0_EIF5);

        /* External Interrupt Status Flag. Write 1 to delete it. */
        SetBit(SIUL2, DIRER0, DIRER0_EIRE5);


1 Reply

1,939 Views
KushalShahNXP
NXP Employee
NXP Employee

Hi Ronald,

You also need to configure MSCM_IRSPRCn register for that interrupt and GIC-400 module.

Moreover, We are now moving to ticketing system to support this device. This community will be closed soon.

For all future questions please raise a service request at www.nxp.com/support using "Support Requests" option and experts will help you with your questions.

 

-Kushal