AnsweredAssumed Answered

Are TX1 and TX2 interchangeable on MFRC630?

Question asked by Rob Helvestine on May 14, 2018
Latest reply on Jun 4, 2018 by Estephania Martinez

I have a design that requires the antenna matching circuitry to be on the opposite side of the board than the MFCR630. Can I swap TX1 and TX2 so that routing is easier and those nets don't have to cross? See the two schematics below.

 

 

 

Are both of these circuits equally valid? I would assume so as they are symmetric but wanted confirmation. Thanks! 

Outcomes