I've installed NFC Cockpit v4.7.0 and plugged in my CLRC663 dev board, but it always says "Disconnected" in the upper left. How do I reinstall the drivers, as I'm assuming that's my problem. Any other tips? Thanks.
Hi, which BIN File should I use, when working with PNEV7462C?
Hello,
Please refer to the following community thread:
https://community.nxp.com/message/1007043
If you have any doubt, please let me know.
Regards,
Ivan.
Hello IvanRuiz,
To clarify, I need to download the MCUXpresso IDE, and use that to flash that binary onto the cockpit hardware? Is that correct?
I can't seem to download the MCUXpresso IDE. See the error message below when I click on "download"
Any help?
Also IvanRuiz,
Here is my log screen when I plug in the Cockpit tool:
Just want to make sure there is nothing else preventing me from using the tool. Thanks.