AnsweredAssumed Answered

Display Support

Question asked by Abhinandan Singh Rawat on May 11, 2018

Hi 

 

I am using IMx6 Quad processor . 

 

I want to drive two outputs to support two displays.

 

Outputs are : 

  • VGA
  • DisplayPort

 

Inputs are :

  • LVDS 1 Port: 170 Mpixels/Sec or LVDS x 2 ports: 85 Mpixels/sec
  • HDMI 1.4 a
  • RGB 24 Bit 266 Mpixels/sec

 

Resolution : 1920 x 1080 @ 60 Hz.

 

Please recommend an approach on how can I simultaneously drive both displays via VGA and a DisplayPort .

 

I believe single LVDS cannot support such HD resolution and thus I will be needing to use 2 LVDS for it. 

 

Still, anyone giving any leads will be highly appreciated. 

 

 

Thanks

Outcomes