I am studying the schematic of the new (A1) version of the RT1050 EVK board.
The schematic shows the signal ENET_CRS_DV coming from the PHY to MCU pin C12, which is described as "ENET_RX_EN". On the other hand, signal ENET_INT goes to G13, which can be associated to ENET_CRS.
So I wonder if these two signals are swapped, or if there is something I am missing (quite possible, I'm not an expert of Ethernet).
Hints and suggestions?
Giuseppe
Hi Giuseppe
for names of rmii signals and its usage may be useful also to look
How to use i.MX6SDL ENET_CRS_DV pad for CRS for RMII mode.
I think there is no swapping, ENET_INT is handled processor as gpio interrupt.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------