AnsweredAssumed Answered

gateway SDcard boot issue : Bad Linux ARM zImage magic

Question asked by Angeliki Leonida on May 9, 2018
Latest reply on May 10, 2018 by Angeliki Leonida

Hi, 

 

I created an SD card image  for the gateway by following the instructions in 'MGSBIUG.pdf(1.4.0)'. The only addition  in the image is a meta-mono layer. 

I get an error when booting from the SDcard. Though i managed to manually boot the image manually providing commands in uboot. 

 "run loadimage;run mmcboot"

 

can you please help debug ? 

 

Error during boot: 

U-Boot 2017.03-nxp/imx_v2017.03_4.9.11_1.0.0_ga+ga2fea67 (Apr 26 2018 - 16:26:47 +0300)

CPU: Freescale i.MX6UL rev1.1 528 MHz (running at 396 MHz)
CPU: Commercial temperature grade (0C to 95C) at 48C
Reset cause: POR
Model: Freescale i.MX6UL Volansys Gateway
Board: MX6UL Volansys Gateway
I2C: ready
DRAM: 256 MiB
PMIC: PFUZE3001 DEV_ID=0x31 REV_ID=0x11
NAND: 1024 MiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1
*** Warning - bad CRC, using default environment

In: serial
Out: serial
Err: serial
Net:
Warning: ethernet@02188000 using MAC address from ROM
eth0: ethernet@02188000 [PRIME]
Normal Boot
Hit any key to stop autoboot: 0

NAND read: device 0 offset 0x4000000, size 0x800000
8388608 bytes read: OK

NAND read: device 0 offset 0x5000000, size 0x100000
1048576 bytes read: OK
Bad Linux ARM zImage magic!
=>

 

 

Outcomes