Dear Technical support team,
1. I would like to know what is the units of the ADC's sampling frequency listed in the sysfs entries,
By default I see the sampling frequency as 58098 , Is that the 58098 is 58.098KHz or what is the units of 58098???
Kindly let me know what is units of the the below values as well
cat sampling_frequency_available
206250 58098 29676 15000 7541
2.
As am stuck in finding the units from past many days, kindly do the needful as early as possible
Hi Sri
please check linux documentation sysfs-bus-iio
sysfs-bus-iio\testing\ABI\Documentation - linux-imx - i.MX Linux kernel
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------