AnsweredAssumed Answered

i.MX6: Yocto with OpenCL

Question asked by concerned12345 on May 3, 2018
Latest reply on May 3, 2018 by igorpadykov

I have a Yocto build with core-image-minimal and I'd like to be able to add OpenCL. I do not want Qt or any image with Qt since this will bloat my image. I've already tried the following while keeping core-image-minimal:

https://community.nxp.com/thread/446633

https://community.nxp.com/thread/428397

After building I do not have any RPM package for OpenCL or any of its libraries as stated in the above threads. It seems the only way to add this is to create an image with Qt (i.e. fsl-image-qt5).

 

Is there a way to add OpenCL with the Vivante drivers to core-image-minimal so I can keep my image as small as possible?

Outcomes