iMXRT1050-EVK SDK vs iMXRT1050-EVKB SDK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMXRT1050-EVK SDK vs iMXRT1050-EVKB SDK

1,523 Views
steve_n
Contributor II

As far as I can tell, I have an IMXRT1050-EVK (not B) - yet, when I go to build an SDK, it only references EVKB under boards supported. I attached a screen shot highlighting what I am referring to. Is the SDK for EVKB backward compatible or no?

I originally didn't think anything about it, but after reading this thread  iMXRT1050-EVKB runtime difficulties with project based on EVKB SDK v2.3.1‌ I'm wondering if I am experiences issues related to this.

I am able to download programs however I cannot debug them. The debugger seems to silently detach and hang and when I try to stop the debugger, MCUXpresso stops responding until I kill the GDB server.

I am using PE Micro's Multilink Universal FX.

0 Kudos
2 Replies

983 Views
2winkle
Contributor III

Hello steve_n‌,

I am using PEMicro Multilink Universal debugger.

I too have the same problem. However, I am able to debug by running it again.

After programming, restart the iMXRT board. Then debug using the 'Attach on running target' option. That should enable you to debug using the debugger.

ydfyh.png

0 Kudos

983 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Stephen Noonan,

It seems the Multilink Universal FX doesn't support programing  code into hyperflash of  RT1052 ,

I using it test on IMXRT1050-EVKB board, also failed.

Please use the on board debugger  , DAP-LINK firmware . Or LPC-link2.

https://community.nxp.com/message/971721 

BR

Alice

0 Kudos