Hello, Sir:
I use mfgtool for i.mx8mq-evk and it works fine under windows.
But when I try to use mfgtool (from L4.9.51_8mq-ga_mfg-tools) i.mx8m-evk under linux, i get failed code#24.
The command i issue is as below:
$ ./linux-runvbs.sh mfgtool2-yocto-mx8-evk-emmc1.vbs
mfgtool2-yocto-mx8-evk-emmc1.vbs
Executing: ./mfgtoolcli -l eMMC -s mmc=0
Your Options:
mmc: 0
Ready to flash.
init op Failed code# 24$ cat MfgToolLibLog.txt
DLL version: 2.3.4
Wed Apr 25 16:49:08 2018
Start new logging
ModuleID[2] LevelID[1]: Error: Invalid device name: MX8QM
ModuleID[2] LevelID[1]: Parse ucl script failed, error code: 24
Is i.mx8mq supported in mfgtool under linux?
Thank you~
the mfgtool official website released is for windows, for linux version, pls refer to the discussion as below:
https://community.nxp.com/message/933750?commentID=933750#comment-933750