AnsweredAssumed Answered

Device not responding, but it works in one direction.

Question asked by zafer sen on Apr 24, 2018
Latest reply on Apr 25, 2018 by zafer sen

Hi,I have a Volansys Modular Gateway.

I am working on example code, but I'm facing a different error. My MENP-KW41Z and FRDM-KW41Z modules are successfully connected to the gateway and the Android application is notified that the devices are online. However, when I click on the active devices through the application, I get a device not responding. However, when I click on SW2 or SW3 button from MENP or FRDM devices, it shows how many times I click the buttons on the android application, but I can not send commands to the devices via the android application either. What could be the reason for this error?

Outcomes