AnsweredAssumed Answered

MK66FN2M0VLQ18 ADC DIFF. Inputs

Question asked by John Cooper on Apr 23, 2018
Latest reply on Apr 25, 2018 by Fang Li

Hello,

 

I have a question about the MK66FN2M0VLQ18s ADC. I am using an applications that requires at least 2 but possibly 3 differential ADC Inputs. The MK66FN2M0VLQ18 reference manual eludes to there being up to 4 differential ADC inputs but the MK66FN2M0VLQ18 datasheet  has only 3 pins labels with DM marker and one is an overlap between the two diffent input channels, meaning I can at best only use one differential ADC input. Is this right or is there something I am missing like some of the single ended inputs can be used as well.

 

Thanks,

John

Outcomes