s12zvl32芯片的stop mode 电流 问题

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

s12zvl32芯片的stop mode 电流 问题

1,195 Views
zhou
Contributor III

s12zvl32芯片的stop mode 电流 问题

我现在用s12zvl32进入stop mode ,电流在200uA。手册上写的可以低于100uA

pastedImage_1.png

pastedImage_2.png

是否是哪个模块没有关闭?

目前我测试,程序里面直接进入stop mode,前面不做任何设置,也是200uA左右。

硬件上的话,就是把 VDDX和VDDA直接相连,其它引脚我都断开连接了。

有没有相关的资料可以参考?

0 Kudos
2 Replies

1,039 Views
zhou
Contributor III

pastedImage_1.png

主要是E和J口,有六个是默认PULL DEVICE,导致有150uA的电流消耗。

当然,如果用了ADC功能,就如上面的兄弟说的,要把ADC的模块重启(soft-restart)下,在进入stop mode前,不然会有500uA左右的多余电流消耗。

0 Kudos

1,039 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,
Do you use ADC in your project?
Please see Mask Set Errata for Mask 0N22G – Errata

e8188: ADC: High current in Stop Mode

Is the MCU entering Full-stop mode or Pseudo-stop mode?

Make sure that none of the pins is floating.

Regards,
Daniel