OM13092 LPCXpresso54608 Out of box Demo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OM13092 LPCXpresso54608 Out of box Demo

764 Views
richardlai
Contributor I

Hi

Does anyone know where can I download the source/binary of the out-of-box demo ("Draupner" I believe)? I recently purchased this dev kit (OM13092 - LPCXpresso54608), which has this particular demo preloaded. which is also the one showcase on the official get started guide and video. However, I am not able to find the source/binary of this demo.

 

There seems to have another newer(?) demo for this board called Sprinkler, which binary and source are available on https://touchgfx.com/nxp-semiconductors/lpc5460x/. I have trouble compiling this demo though, which after following instructions in "TouchGFX NXP LPC54608 Board Support Package - Installation V1.5" pdf, I get the following error message:

 

make: *** No rule to make target `C:/nxp/TouchGFX_NPX_LPC54608_BSP/touchgfx/os/FreeRTOS8.2.0/OSWrappers.cpp', needed by `TouchGFXPort/OS/OSWrappers.o'.  Stop.

 

The BSP I downloaded from the link https://touchgfx.com/nxp-semiconductors/lpc5460x/ simply does not contain OSWrappers.cpp file. I don't know whether is the installation document or BSP not updated. The SDK version I generated and downloaded from "MCUXpresso SDK Builder" is 2.3.1, and software components I have selected are: CMSIS DSP Library, USB stack, lwIP, FreeRTOS.

May be the Sprinkler BSP is no longer supported with the latest SDK version, or latest SDK has broken the demo source. I have no idea where to get/generate older version of SDK for LPCExpresso54608. This is my first time using NXP platform.

BR/Richard

Labels (1)
0 Kudos
1 Reply

473 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Richard,

I managed to flash the new demo in the LPCXpresso54608. When you download the files from the next page https://touchgfx.com/nxp-semiconductors/lpc5460x/ you have a .axf file I convert this file to .hex with the help of MCUXpresso. To do this please copy the .axf file into any workspace that you have open

pastedImage_1.png

Then right click on the file > binary utilities > create hex

pastedImage_2.png

Once you have the .hex file of the demo you can follow the steps of the guide attach. 

You can follow this steps for the moment. Meanwhile I will see if it's possible to upload to our page the files of the old demo.  

Hope it helps!

Victor.

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos