Hello, I am new on Freescale. I am surprise Codewarrior will be installed only in virtual machine Windows XP, not in a usual Windows 64 bit like Win7. Is this real?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hello, I am new on Freescale. I am surprise Codewarrior will be installed only in virtual machine Windows XP, not in a usual Windows 64 bit like Win7. Is this real?

739 Views
henryscott
Contributor I

Hello, I am new on Freescale. I am surprise Codewarrior will be installed only in virtual machine Windows XP, not in a usual Windows 64 bit like Win7. Is this real?

0 Kudos
4 Replies

505 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Henry,

Could you tell us which MCU are you using? If you are not using a legacy device there should be a new CodeWarrior version that supports Win 7.

Thanks in advance!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 Kudos

505 Views
henryscott
Contributor I

I am using this

MC9S08SE8VWLE

Thank you nd best regards

Henry

Il 23/04/2018 22:19, Carlos_Mendoza ha scritto:

>

NXP Community

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

>

Re: Hello, I am new on Freescale. I am surprise Codewarrior will

be installed only in virtual machine Windows XP, not in a usual

Windows 64 bit like Win7. Is this real?

reply from Carlos_Mendoza

<https://community.nxp.com/people/Carlos_Mendoza?et=watches.email.thread>

in /CodeWarrior for MCU/ - View the full discussion

<https://community.nxp.com/message/1008077?commentID=1008077&et=watches.email.thread#comment-1008077>

>

0 Kudos

505 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Henry,

 

For the MC9S08SE8 devices you can use CodeWarrior for MCUs (Eclipse IDE), which comes with host operating system support for Win XP, 7, 8, 8.1 and 10:

CodeWarrior for Microcontrollers-Eclipse IDE|NXP 

 

Hope it helps!

 

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 Kudos

505 Views
henryscott
Contributor I

Ok I see now on my Win7.

Other question, I have Multilink Universal , is there a simle software

like programmer for hex files?

thanks

Henry

Il 24/04/2018 16:15, Carlos_Mendoza ha scritto:

>

NXP Community

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

>

Re: Hello, I am new on Freescale. I am surprise Codewarrior will

be installed only in virtual machine Windows XP, not in a usual

Windows 64 bit like Win7. Is this real?

reply from Carlos_Mendoza

<https://community.nxp.com/people/Carlos_Mendoza?et=watches.email.thread>

in /CodeWarrior for MCU/ - View the full discussion

<https://community.nxp.com/message/1008377?commentID=1008377&et=watches.email.thread#comment-1008377>

>

0 Kudos