imx6q mipi bus allowed signal voltage level

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6q mipi bus allowed signal voltage level

Jump to solution
527 Views
sunjianxin66
Contributor II

Dear NXP

The NVCC_MIPI is recommended as 2.5V from datasheet. I have a camera that outputs 1.8V mipi signals. Can I directly connect those bus signal together? Is a voltage shifter needed? Thank you very much! Please refer the attachment for the mipi signals in schematic screen shot. 

Jianxin

Labels (1)
0 Kudos
1 Solution
441 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jianxin

please check Table 68. Electrical and Timing Information

in sect.4.12.12 MIPI D-PHY Timing Parameters i.MX6DQ Datasheet

http://www.nxp.com/docs/en/data-sheet/IMX6DQCEC.pdf


Best regards
igor
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
442 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jianxin

please check Table 68. Electrical and Timing Information

in sect.4.12.12 MIPI D-PHY Timing Parameters i.MX6DQ Datasheet

http://www.nxp.com/docs/en/data-sheet/IMX6DQCEC.pdf


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos