This is strange....
the busclock is running @ 8MHz
- MTIM enabled 1ms Period
- Serial RX and TX (RIE=1 TIE=1) enabled 9600BD
everything running fine.
When I force a Watchdog-Reset, the System resets but the MTIM is not running anymore!
I had no idea what to do so i tried the CW-Plugin Device initialization.
Same settings as above, Busclock @8MHz but accidentally I forgot to enable the serial RX/TX.
Watchdog reset and the system is running fine.
Then I enabled the serial RX/TX lines and there it is again, the same problem as described above.
Then I reconfigured the CPU to a Busclock @4MHz and reconfigured the peripherials
(MTIM 1ms, Serial 9600BD ...) everything running fine again.
When I force a Watchdog-Reset, the System resets and the MTIM running!!!
System is O.k. Im fine for now, but what the hell is this?!?!