imx8-prg 56070000.prg: unsupported crop line 720 for modifier 0x0000000000000000

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8-prg 56070000.prg: unsupported crop line 720 for modifier 0x0000000000000000

630 Views
shalanyang
Contributor II

HI ,

    we are use imx8qxp ,when I use lvds show logo,the picture can show ,but have some error msg,follow:

    
[ 9.715977] imx8-prg 56070000.prg: unsupported crop line 720 for modifier 0x0000000000000000
[ 9.785750] imx8-prg 56070000.prg: unsupported crop line 720 for modifier 0x0000000000000000
[ 9.851739] imx8-prg 56070000.prg: unsupported crop line 720 for modifier 0x0000000000000000
[ 9.917742] imx8-prg 56070000.prg: unsupported crop line 720 for modifier 0x0000000000000000
[ 9.983571] imx8-prg 56070000.prg: unsupported crop line 720 for modifier 0x0000000000000000
[ 10.049798] imx8-prg 56070000.prg: unsupported crop line 720 for modifier 0x0000000000000000
[ 10.116146] imx8-prg 56070000.prg: unsupported crop line 720 for modifier 0x0000000000000000

I found it print in drivers/gpu/imx/imx8_dprc.c 

void prg_configure(struct prg *prg, unsigned int width, unsigned int height,
unsigned int x_offset, unsigned int y_offset,
unsigned int stride, unsigned int bits_per_pixel,
unsigned long baddr, u32 format, u64 modifier,
bool start)

{

...............

if (y_offset >
((format == DRM_FORMAT_NV21 || format == DRM_FORMAT_NV12) ?
(PRG_HANDSHAKE_8LINES - 1) : (PRG_HANDSHAKE_4LINES - 1))) {
dev_err(prg->dev,
"unsupported crop line %d for modifier 0x%016llx\n",
y_offset, modifier);
return;
}

.......

}

BSP Version: body#

imx_4.9.51_8qxp_beta

why have this errr msg?

TKS

0 Kudos
3 Replies

430 Views
shalanyang
Contributor II

HI ,igorpadykov,

      Sorry ,we use the BSP Version is L4.9.51_8qm-beta2/8qxp-beta ,the problem is exist ?can you help me?

      

0 Kudos

430 Views
igorpadykov
NXP Employee
NXP Employee

Hi shalan

please try beta2 release, follow suggestion on

How to enable the HDMI for IMX8 QXP MEK with LVDS to HDMI converter 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

430 Views
shalanyang
Contributor II

IMX8QXP 

0 Kudos