frdmk64f_usb_examples_host_cdc_bm

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

frdmk64f_usb_examples_host_cdc_bm

590 Views
elinaiman
Contributor I

I created the frdmk64f_usb_examples_host_cdc_bm project. How do I test it. Does it use usb0 or usb1. Can I use usb0 to power the board and usb1 to echo back the data.

Where is the code that echos back the characters.

0 Kudos
1 Reply

496 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Eli Naiman

It seems your project is the under SDK package, there is a "readme.pdf",

it describe the detail steps about how to configure boards and run project :

\SDK_2.3.0_FRDM-K64F\boards\frdmk64f\usb_examples\usb_host_cdc\bm

Hope it helps


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos