AnsweredAssumed Answered

Two questions about S912XEP100W1MAL

Question asked by Bin Huang on Apr 11, 2018
Latest reply on Apr 13, 2018 by ZhangJennie

I have tow questions abou S912XEP100W1MAL ,could you help to check

 

1, There have some contents in the PRM file of XEP100,as follow,I need to use ROM_4000,but failed,error information such as picture 1 in attachment, 

 

COPY                    /* copy down information: how to initialize variables */

                              /* in case you want to use ROM_4000 here as well, make sure

                                 that all files (incl. library files) are compiled with the

                                 option: -OnB=b */

                        INTO  ROM_C000/*, ROM_4000*/;

 

2.The _Startup address is 16 bits in the map file of XEP100 ,the interrupt vector address is also 16 bits in the S19 file,

 

But assigning value must be long integers, otherwise there will be a mistake as picture 2 ,picture 3 ,picture 4

Attachments

Outcomes