maximum system clock settings

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

maximum system clock settings

841 Views
matthiaspimming
Contributor I

Hello, I'm looking for the maximum system clock settings on the i.MX RT 1050.

I found the Table 18-4 System Clock Frequency Values in chapter 18 on page 694 in the Reference Manual ( (https://www.nxp.com/docs/en/reference-manual/IMXRT1050RM.pdf ).

It says that the maximum frequenzy for IPG_CLK_ROOT for example is 150MHz. But in the example projects it is set to 300MHz. There is no detail descripton of Table 18-4 in the reference manual. What does that mean?

Thanks.

Labels (1)
0 Kudos
1 Reply

713 Views
joanxie
NXP TechSupport
NXP TechSupport

what example project do you mean? could you tell me the detailed project name? let me double check it

0 Kudos