c'est un lpc 2134fbd01 faudrait-il peut etre un schema du kit transistore a relier avec ulink 2 chinois pour que celui ci detecte ce prosseceur ?merci de me fournir ce schema
thank you victor for your answer but must i clarify that my ulink 2 is a chinese clone and i need an exact scheme of the resistances that i need to add and where to put the debug jump to connect the whole
I did not understand well on the schema of the link that you gave me I thought I saw a logical circuit ic2 ic4 ic5 ic6 ic6 I do not see which one and then that mean
Here is a schematics of JTAG interface circuits that are part of ULINK2:
http://www.keil.com/support/man/docs/ulink2/ulink2_hw_schematic.htm
Have a great day,
Victor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------