Hi,
I am trying to configure the I2S interface to use with pll but unfortunately isn't working. I am not sure what I am doing wrong. I have looked at the example within the SDK but the drivers in there have different functions to the ones I have, for instance in the SDK example there is a slm_clock.c file which has all the functions to configure the I2S with pll (enable clock peripherals attach clock peripherals etc..); instead I have two different files (pll_5460x.c and clock_5460.c) with different functions to the ones in the example.
This is what I currently have:
/* PLL data for input = 12 MHz */
static const AUDPLL_SETUP_T pll_setup_48KHz = {
0x00007C40,
0x0000002D,
0x0000001B,
0x0002074,
0x00800000,
24576000,
0 * PLL_SETUPFLAG_WAITLOCK, /*!< PLL setup flags, Or'ed value of PLL_SETUPFLAG_* definitions */
};
Chip_Clock_SetAudioPLLSource(SYSCON_AUDPLLCLKSRC_FRO12MHZ);
Chip_Clock_SetAudioPLLFreq(&pll_setup_48KHz);
Chip_Clock_EnablePeriphClock(SYSCON_CLOCK_IOCON);
Chip_IOCON_PinMuxSet(LPC_IOCON, 3, 11, (IOCON_FUNC1 | IOCON_MODE_INACT | IOCON_DIGITAL_EN));
Chip_Clock_DisablePeriphClock(SYSCON_CLOCK_IOCON);
Chip_Clock_SetMCLKClockSource(SYSCON_MCLKSRC_AUDIOPLL, 1);
Any help would be really appreciated.
Hi Jacinto Moreno ,
You can configure the clock source for I2S visually by using the MCUXprsso Congig Tools which can generate the related code too.
Please clicking the following link to access the on-line tool
Welcome | MCUXpresso SDK Builder