Bret Liu @CarlosCasillas
We are using ADV7482 on our board with iMX6Q and I am trying to modify ov5642_mipi.c for adv7482_mipi_tvin.c. I have two questions when I modified the driver.
I use Bsp is L3.0.35_linux.
when I try ./mxc_v4l2_overlay.out -iw 720 -ih 576 -ow 1024 -oh 768 -m 4 -bg
I hope to get your help.,thanks
Questions as follows
this is log:
ERROR: unrecognized std! 59565955 (PAL=ff, NTSC=b000
RGB565
frame buffer width 1024, height 768, bytesperline 2048
imx-ipuv3 imx-ipuv3.0: IPU Warning - IPU_INT_STAT_5 = 0x00000001
imx-ipuv3 imx-ipuv3.0: IPU Warning - IPU_INT_STAT_5 = 0x00000001
imx-ipuv3 imx-ipuv3.0: IPU Warning - IPU_INT_STAT_5 = 0x00000001
imx-ipuv3 imx-ipuv3.0: IPU Warning - IPU_INT_STAT_5 = 0x00000001
imx-ipuv3 imx-ipuv3.0: IPU Warning - IPU_INT_STAT_5 = 0x00000001
imx-ipuv3 imx-ipuv3.0: IPU Warning - IPU_INT_STAT_5 = 0x00000001
imx-ipuv3 imx-ipuv3.0: IPU Warning - IPU_INT_STAT_5 = 0x00000001
imx-ipuv3 imx-ipuv3.0: IPU Warning - IPU_INT_STAT_5 = 0x00000001
how about try to use mxc_v4l2_tvin.out? it seems de-interlacing issue