I'm looking at implementing firmware updates over an ethernet connection on a MKV58F1M. I can get my application to receive and store an update file into the internal flash. Is there a way to launch the bootloader such that it performs an update from a known location in the internal flash?
Solved! Go to Solution.
Hi,
In general, the bootloader routine located from internal Flash boot up address (0x0).
If there with suitable application code, after the chip boot up, the bootloader will jump to application code.
Customer could check here about Kinetis Ethernet bootloader demo for reference.
Wish it helps.
Have a great day,
Mike
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
In general, the bootloader routine located from internal Flash boot up address (0x0).
If there with suitable application code, after the chip boot up, the bootloader will jump to application code.
Customer could check here about Kinetis Ethernet bootloader demo for reference.
Wish it helps.
Have a great day,
Mike
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------