We're considering using K64F for an application requiring TCP/IP (DHCP, RFC2217, possibly http).
Is there a network example for Freedom FRDM-K64F board using FreeRTOS? Erich posted an example some years ago but that uses (deprecated) processor expert and KDS...
Thanks!
Hi Dave,
Check my GitHub --> github.com/IceDefcon
You will find FreeRTOS.LWIP project implemented on K64F. Just need to download arm-none-eabi-gcc and compile it
In my case under Ubuntu.18.04.3 LTS with 5.0.0-29-generic
Enjoy,
Ice
Wow, a reply to a year-and-a-half old post!
We're not developing with NXP at the moment, though I am using LwIP 2.1.2 in another FreeRTOS project.
Thanks though,
Best Regards, Dave
I found frdmk64f_demo_apps_lwip_lwip_httpsrv_freertos. I'll give this one a try...
Hi Dave:
There are several tcpip demos under folder lwip, most of them with freeRTOS.
Regards
Daniel